Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

What is the smallest package in H8/Tiny Series?

Latest Updated:03/24/2009

Question:

What is the smallest package in H8/Tiny Series?

Answer:

LQFP and QFN packages are minimum dimension which is7mmx7mm, QFN is the smallest on Implement area.
Suitable Products
H8/300H Tiny
H8/36014, H8/36024
H8/3694