Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

What value is in free blank area of PROM, Flash Memory and QzROM version?

Latest Updated:12/01/2005

Question:

(ROM)  What value is in the free blank area of shipped blank one-time PROM, Flash Memory and QzROM versions? [2005/12/01]

Answer:

"FFh" is set. (#104909)
Suitable Products
3803H
3803L
3823
3850A
3858
38D2
38D5
7544
7545
7546
7547
7548
7549