Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Why does one byte of unintended data is sent in UART mode?

Latest Updated:01/11/2008

Question:

In UART mode, if the UiRB register is read after data is received, one byte of unintended data is sent. Why is this?

Answer:

Continuous receive mode might be enabled.
In continuous receive mode, the TI bit in the UiC1 register becomes 0 (data in UiTB register) by reading of the UiRB register.
Set the UiRRM bit to 0 (disables continuous receive mode) in UART mode.
Suitable Products
R8C/18
R8C/19
R8C/1A
R8C/1B
R8C/20
R8C/21
R8C/22
R8C/23
R8C/24
R8C/25
R8C/26
R8C/27
R8C/28
R8C/29
R8C/2A
R8C/2B
R8C/2C
R8C/2D
R8C/2E
R8C/2F
R8C/2G
R8C/2H
R8C/2J
R8C/2K
R8C/2L
R8C/32C
R8C/33C
R8C/35C
R8C/36C
R8C/38C
R8C/3GC
R8C/3JC
R8C/32D
R8C/33D
R8C/35D
R8C/3GD
R8C/33T
R8C/38A
R8C/34E, R8C/34F, R8C/34G, R8C/34H
R8C/36E, R8C/36F, R8C/36G, R8C/36H
R8C/38E, R8C/38F, R8C/38G, R8C/38H