Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Are the Standard and Professional editions different compilers?

Last Updated:05/17/2017

Question:

Are the Standard and Professional editions different compilers?

Answer:

The compiler is the same. The only difference is the license registered on the PC.

The license is checked at the time of compilation. If a license for the Professional edition is registered, you can use the dedicated features of that edition.

Suitable Products
C Compiler Package for RH850 Family
C/C++ Compiler Package for RX Family
C Compiler Package for RL78 Family
  • Was this article helpful?