Skip to main content
Renesas India - Knowledgebase

F0563100 message (CC-RL)

Last Updated:06/07/2017


I am using RL78 Compiler CC-RL. The following error message appears. How do I resolve this?

F0563100:Section address overflow out of range : "section"


The section allocation address may be out of the available range because many program codes, data items, and variables are assigned to the section.

Check the memory mapping of the devices you are using, and then review the program codes, data, and variables you are using, or adjust the start address of the section by using the -start option so that the section falls within the ROM or RAM area.

You can check the section size for each source file in the section list information of the assemble list file. (The size in the section list information might be different from that for the actual allocation depending on the arrangement conditions and others.)

Refer to the user’s manual for details of the section list information.

- 3.1.3 Section list information in the CC-RL Compiler User's Manual

Suitable Products
e² studio
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 Family
  • Was this article helpful?