Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Is it possible to change the server PC for a floating license?

Last Updated:08/30/2017

Question:

Is it possible to change the server PC for a floating license?

Answer:

Yes, you can easily uninstall the software from an old server PC, re-install it on a new PC, and then change the settings of the client PCs. Refer to the following manual for the methods of installation and setting.

Floating License Server V2.01.00 User's Manual

Suitable Products
C Compiler Package for RH850 Family
C/C++ Compiler Package for RX Family
C Compiler Package for RL78 Family
  • Was this article helpful?