Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Is it possible to check the usage of a floating license?

Last Updated:05/17/2017

Question:

Is it possible to check the usage of a floating license?

Answer:

You can check it with the floating license server management dialog on the server PC.
You can also make an optional setting for the output of the data to a log file for later checking.
Suitable Products
C Compiler Package for RH850 Family
C/C++ Compiler Package for RX Family
C Compiler Package for RL78 Family