Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Upgrading Standard Edition of Annual License

Last Updated:11/29/2017

Question:

Can I upgrade the Standard edition of annual license to the Professional edition (available for one year) by using the upgrade edition of permanent license?

Answer:

No, you cannot. The upgrade editions upgrade Node Locked permanent licenses only.
Suitable Products
C Compiler Package for RH850 Family
C/C++ Compiler Package for RX Family
C Compiler Package for RL78 Family
  • Was this article helpful?