Skip to main content
Renesas India - Knowledgebase

W0561017 Message_CC-RL

Last Updated:12/06/2017


I am using RL78 compiler CC-RL. I got the following warning message. What should I do?

“W0561017: The evaluation period has expired”


The message appears because the free evaluation period has expired as 60 days or more have passed after the first build of CC-RL V1.xx.xx.
Therefore, if you have purchased a compiler product, register the license key accompanied with the product in the license manager.
Suitable Products
e² studio
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 Family
  • Was this article helpful?