Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

W0561100 message (CC-RL)

Last Updated:06/07/2017

Question:

I am using RL78 Compiler CC-RL. The following error message appears. How do I resolve this?

W0561100:Cannot find "section-name" specified in option "start"

Answer:

Although the section name output in the message is specified with the -start option of the linker, that section does not exist, and therefore the message appears.

Check whether the section name specified for the option is correct.

Note that when you use #pragma section in a C source file, "_n" or "_f" is suffixed to the generated section name.

Suitable Products
e² studio
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 Family
  • Was this article helpful?