Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

W0561120 Message(CC-RL)

Last Updated:04/17/2017

Question:

I am using the CC-RL compiler for RL78 devices. What should I do in response to the error message below? 
WO561120: Section address is not assigned to “section name”

Answer:

This message appears when the -start option of the linker has not been specified for the section for which the message is displayed. 
Specify the -start option for the given section.
Suitable Products
e² studio
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 Family
  • Was this article helpful?