Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

(E1,E20) I clicked “Do not show this dialog box again” and I want it shown again.

Latest Updated:12/01/2010

Question:

When I connect E1 or E20 to the user system, the [Initial Settings] and [Configuration Properties] dialog boxes are no longer displayed. How do I get these dialog boxes to be displayed again?

Answer:

To display the [Initial Settings] dialog box, follow either of the steps listed below.

  • Connect E1 or E20 while pressing the Ctrl button on the keyboard.
    This will open the [Initial Settings] dialog box.
  • After connecting E1 or E20, select [Setup] → [Emulator] → [Device Setting] from the menu.
    Open the [Initial Settings] dialog box and remove the tick mark in front of “Do not display this dialog box at startup” at the bottom of the box.
    This will ensure display of the [Initial Settings] dialog box at the next startup.

To display the [Configuration Properties] dialog box, follow either of the steps listed below.

  • When connecting E1 or E20, click the OK button in the [Initial Settings] dialog box while pressing the Ctrl button on the keyboard.
    This will open the [Configuration Properties] dialog box.
  • After connecting E1 or E20, from the menu select [Setup] → [Emulator] → [System].
    Open the [Configuration Properties] dialog box and remove the tick mark in front of “Do not display this dialog box at startup” at the bottom of the box.
    This will ensure display of the [Configuration Properties] dialog box at the next startup.
Suitable Products
E1 [R0E000010KCE00]
E20 [R0E000200KCT00]