Skip to main content
Renesas India - Knowledgebase

Can the user controller be used when debugging E10A-USB?

Latest Updated:08/07/2008


Can the user break controller that is built-in to the target MCU be used while when debugging with E10A-USB?


SH2, SH2A, SH7750 and H8SX Family MCUs: (excluding SH7606, SH7618, and SH7619)

No, the user break controller can not be used while debugging with E10A-USB.

All other SH Family MCUs:
Yes, the user break controller can be used, but the emulator functions will be limited to the following:

Event condition, performance measurement function, profile function, step commands, trace function.
*Note: limitations differ according to MCU product.

For more details refer to the E10A-USB Help File for the target MCU.
Suitable Products