Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Error (E0210002) occurs when connecting MCU and E1

Last Updated:01/24/2018

Question:

I get a connection error with E0210002 error message on the CS+ for CC when connecting a MCU and the E1. How can I resolve this?

[Direct Error Cause]

Could not load file or assembly 'QEInformation, Version=1.0.0.0, Culture=neutral, PublicKeyToken=3e0e6d2b80718d7e' or one of its dependencies. The system cannot find the file specified.

Answer:

Install the CS+ QE, which is necessary for debugging on the CS+ V4.00.00 or later.
The CS+ supports Smart Utility and QE (Quick and Effective tool solution), which are advanced development environment tools.

Download the suitable CS+ QE module for the CS+ which you are using.

To download the latest versions of CS+ and CS+ QE, click here.

To download the earlier versions of CS+ QE, click here.

The module can be installed automatically by auto-updating according to an upgrade of CS+ (the common programs). However, if the module is not installed automatically, download it by the preceding way. After installation, restart your PC.

If the above procedure does not work well and you cannot install the module, try to overwrite an existing installation by the installer of the evaluation edition of CS+ for CC.

A compiler is not an evaluation edition when you input a license key.

To download the evaluation edition of CS+, click here.

Suitable Products

E1 [R0E000010KCE00]
E2 Emulator [RTE0T00020KCE00000R]
E20 [R0E000200KCT00]
E2 Emulator Lite [RTE0T0002LKCE00000R]
CS+ (formerly CubeSuite+)
RX Family
RL78 Family
RH850 Family