Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

How to register assembler symbol in watch window

Last Updated:09/27/2017

Question:

I want to register the assembler symbol in the watch window, but it is already set to "int type". How can I specify a different type?

Answer:

Register the assembler symbol in the watch window by specifying the size as shown below. Therefore it can be displayed in the selected size.
Example) To display the assembler symbol VALUE in 8-bit length;
               (char)VALUE

Example) To display the contents of address 0x500 in unsigned char type;
               (unsigned char)0x500

Suitable Products

E8
E200F
E6000
E6000H
E10A-USB
E10T-USB