I cannot get the command to execute HEW
Last Updated:09/27/2017
Question:
After entering a command in the command line window in the High-performance Embedded Workshop, I can't get the command to execute.
(Example: I added the execute command (Go) but I can't execute the program.)
(Example: I added the execute command (Go) but I can't execute the program.)
Answer:
Check to see if the "open bracket indicator" is blinking as shown below.
Try adding "]" to the command line window to terminate the blinking "open bracket indicator".
The "open bracket indicator" blinks when "[" is input to the command line window. In this case, the commands that are input while the indicator is blinking are held until the indicator goes off, and then executed.
Suitable Products
E8 |
E8a |
E200F |
E6000 |
E6000H |
E10A-USB |
E10T-USB |
E100 |
E30A |
PC4701L |
PC4701M |
PC4701U |
PC7501 |