Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Recommended connection example between H-UDI port connector and terminals

Last Updated:10/11/2017

Question:

Can you give me examples of recommended connection method between H-UDI port connector and terminal ?

Answer:

Please refer to the Documentation site of you emulator and find a PDF file of your target device.
If you want to know about any other microcomputers than which listed in the E10A-USB Documentation site, please refer to E10A-USB emulator users manual attached to your E10A-USB emulator.
Suitable Products
E10A-USB