Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

There is no response from MCU. Recover the state by resetting MCU?

Latest Updated:08/27/2010

Question:

[E8a emulator software V.1.04 Release 00 or later]
The message "There is no response from MCU. Recover the state by resetting MCU?" appears, and by clicking on the "OK" button, I can go on debugging, but the same message appears in short time. What is causing this ?

Answer:

The following FAQs may describe the causes of this problem (the same message appears repeatedly).
Make sure the problems and solutions described at "Answer" in the following FAQs.

Suitable MCU FAQ No.
R8C Family FAQ 102357
R32C/100 Series FAQ 102357
M32C/80 Series FAQ 106856
FAQ 102357
M16C/60, /50, /30, /Tiny Series FAQ 102357
FAQ 106856
FAQ 106960
FAQ 107058
740 Family FAQ 102357

Product Concerned : E8a emulator software V.1.04 Release 00 or later

 

Suitable Products
E8a