Skip to main content
Renesas India - Knowledgebase

Why do error occur after software breaks during debug in on chip memory?

Latest Updated:07/17/2008


When I execute a program, which uses DMA transfer, after setting software breaks during debug in the on-chip Flash memory area, the following error is displayed and the emulator will not operate. (SH Family, H8SX Family, H8S Family: on-chip Flash MCU)

Error message: Communication timeout error


A software break occurs when the memory is programmed (replaced with a break command).
During a memory write/erase event, when the CPU enables the bus for a DMA transfer, the MCU goes to the error protect state and the write/erase event in progress is terminated. Therefore, when using DMA transfers use a hardware break that does not program the memory.

For more details concerning the error protect state, refer to the chapter describing the Flash memory in the target MCU hardware manual.

Suitable Products