Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Why does MCU didn't show up in pull down menu of CPU dialog box displayed?

Last Updated:11/01/2017

Question:

The target MCU does not show up in the [CPU Select] pull down menu of the [CPU Select] dialog box displayed at the time the emulator is connected.

Answer:

Suitable Products
E10A-USB