Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Cannot output log data when debugging with sample project using FIT

Last Updated:06/28/2017

Question:

Log data is not output to the debug console in the RI600V4/RI600PX sample project using FIT

Answer:

Log output is disabled by default. To enable log output, follow the steps below.

1. From the CS+ menu, select [Tool], and then [Plug-in Setting...].

2. Select the check box for [Debug Console Plug-in], and then click the [OK] button.

3. In the sample project source file rtos_sample_config.h, remove the comment sign from the following line that is commented out.

  //#define USE_DEBUG_MESSAGE

  Alternatively, specify USE_DEBUG_MESSAGE in the macro definition of the compiler option.

Suitable Products

RI600V4
RI600PX