Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Using the E1 or E20 emulator, is it possible to use the AZ78V4 performance analyzer to obtain a trace display for an application which is using the RI78V4 operating system?

Latest Updated:06/12/2015

Question:

Using the E1 or E20 emulator, is it possible to use the AZ78V4 performance analyzer to obtain a trace display for an application which is using the RI78V4 operating system?

Answer:

No, it is not possible. This is because the AZ78V4 uses a record of data access to obtain a trace display. To use the AZ78V4 in tracing, you need to
•    use IECUBE, or
•    use a simulator.
Suitable Products
RI78V4 V1 Real-time OS for RL78 Family and 78K0R