Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

What happens when an FPU attribute is specified for a task without floating point calculations?

Last Updated:05/17/2017

Question:

Is it OK to specify the FPU attribute "TA_COP1" for a task that does not perform floating point calculations?

Answer:

Yes, it is OK. However, note that it may consume more stack memory and take more time for dispatching, compared to when TA_COP1 is not specified.
Suitable Products
HI7000/4
  • Was this article helpful?