Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Why is an interrupt handler being called repeatedly?

Last Updated:05/17/2017

Question:

Why is an interrupt handler being called repeatedly?

Answer:

The interrupt handler may be called repeatedly until the interrupt factor is cleared.

 

Suitable Products
HI7000/4