Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

"When I execute a build with NC30WA, an error message appears. "

Latest Updated:10/04/2012

Question:

I am developing a system with M3T-MR30/4. When I execute a build with NC30WA, the following error is generated. What is the workaround for this?

L2330 (E) Relocation size overflow :

Answer:

Allocate the following areas without exceeding address 0x1FFF.
(1) MR_RAM_DBG section
(2) Top 2 bytes of the MR_RAM section (only when the sns_dpn service call is used)
Suitable Products
C/C++ Compiler Package for M16C Series and R8C Family [M3T-NC30WA]
M3T-MR30/4 Real-time OS for M16C Series and R8C Family