Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Can't I execute the MM execute file in MS-DOS?

Latest Updated:09/15/2006

Question:

Can't I execute the MM execute file in MS-DOS?

Answer:

No, the execute file for MM V.2.00.20 or earlier cannot be executed in MS-DOS. You will need to use Windows 95/98/Me or Windows NT/2000 Prompt (the DOS window).
MM V.3.00 or later must be executed on Windows 95/98/Me or Windows NT/2000.
 
Suitable Products
Maskfile Converter
4500 Series ROM Ordering
720 Series ROM Ordering
38000 Series ROM Ordering
740/7450/7470 Series ROM Ordering
7600 Series ROM Ordering
7200 Series ROM Ordering
7770 Series ROM Ordering
M16C Family ROM Ordering
R8C Family ROM Programmed Shipment Ordering
QzROM Programmed Shipment Ordering
ASSP ROM Ordering
OSD Controller ROM Ordering