Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Can 4559 Group MCUs programs be assembled using debugger M3T-PD45?

Latest Updated:09/11/2006

Question:

Can programs for 4559 Group MCUs be assembled or debugged using emulator debugger M3T-PD45?

Answer:

Programs can be assembled but not debugged with M3T-PD45.
You will need to use compact emulator M34559T2-CPE or the emulator debugger bundled with M3T-PD45M to debug 4559 Group MCUs.
Suitable Products
M34559T2-CPE
PC4504