Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Deleting creation date in source code in Code Generator Plug-in

Last Updated:08/02/2017

Question:

When I execute code generation, source code creation dates are updated. Can they be deleted?

Answer:

You can set “Creation Date” in the property of Code Generator Plug-in. By selecting “Not Create” for this setting, “Creation Date:” in source codes becomes blank and is not output.
“Create” a creation date(example)
/******************************************************************
* File Name    : r_main.c
* Version      : CodeGenerator for RL78/G13 V2.03.04.01 [11 Nov 2016]
* Device(s)    : R5F100LE
* Tool-Chain   : CA78K0R
* Description  : This file implements main function.
* Creation Date: 2017/03/09
*******************************************************************/
“Not Create” a creation date (example)
/******************************************************************
* File Name    : r_main.c
* Version      : CodeGenerator for RL78/G13 V2.03.04.01 [11 Nov 2016]
* Device(s)    : R5F100LE
* Tool-Chain   : CA78K0R
* Description  : This file implements main function.
* Creation Date:
*******************************************************************/
 
Suitable Products
e² studio
CS+ (formerly CubeSuite+)
Code Generator