Skip to main content
Renesas India - Knowledgebase

Does IO Wizard auto set all ports and pins according to peripheral mode?

Latest Updated:09/04/2009


Does IO Wizard auto set the port direction of external interrupt pins, timer pins, serial and other communication protocol pins, ADC pins as according to peripheral operation mode ?


No. IO Wizard does not do consistency check for user's port direction setting with peripheral operation mode setting. In another words, IO Wizard will not auto change the port direction. User is advised to read and follow the advice comment stated in the config.c file, under the title area of each peripheral setting.
Suitable Products