Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

How to change MCU in PDG2

Last Updated:08/02/2017

Question:

I want to change an MCU in PDG2 in the same manner as CS+ and e² studio. How can I do that?

Answer:

PDG2 does not support MCU changing. To change MCU part number (including ROM/RAM size change), a project needs to be newly created.
Suitable Products
e² studio
CS+ (formerly CubeSuite+)
Code Generator