Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

How to confirm data flash memory in intermediate voltage after writing

Latest Updated:04/04/2014

Question:

In EEPROM emulation library Pack01 for the RL78 family of MCUs, is there any way of confirming (internal verification) that the data flash memory is not at the intermediate voltage after writing?

Answer:

Confirming that no results of writing to data flash memory are at the intermediate voltage is handled by the execution of EEL_Execute function with EEL_CMD_WRITE command
Therefore, the library does not include an individual function and command to handle internal verification.
Suitable Products
Flash Self Programming Libraries
Data Flash Libraries