Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

How to find oscillation stop detection on IO Wizard if its available?

Latest Updated:09/04/2009

Question:

I could not find oscillation stop detection function on IO Wizard although the MCU data sheets stated it is available for my target MCU.

Answer:

Present IO Wizard does not support oscillation stop detection function.
Suitable Products
 
  • Was this article helpful?