Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

How to select extension .hfd with MM V.3.00 Release 1?

Latest Updated:09/15/2006

Question:

I can not select extension ".hfd" (output file of the OSD font editor) with MM V.3.00 Release 1. Please let me know how to do it.

Answer:

V.3.00 Release 2 or later versions now have this feature (selecting .hfd extension).
Please download the newest version.
Suitable Products
Maskfile Converter
4500 Series ROM Ordering
720 Series ROM Ordering
38000 Series ROM Ordering
740/7450/7470 Series ROM Ordering
7600 Series ROM Ordering
7200 Series ROM Ordering
7770 Series ROM Ordering
M16C Family ROM Ordering
R8C Family ROM Programmed Shipment Ordering
QzROM Programmed Shipment Ordering
ASSP ROM Ordering
OSD Controller ROM Ordering