Skip to main content
Renesas India - Knowledgebase

Is size of library fixed in user's manual of RL78 FDFL Type04 ?

Latest Updated:04/04/2014


Is the size of the library described in user’s manual of RL78 Family Data Flash Library Type04 fixed?


No, it isn’t.
The size described in the manual is for the case when all functions including the PFDL_GetVersionString function (the function for acquiring the version information of Data Flash Library Type04) are in use.
Not using the PFDL_GetVersionString function of Data Flash Library Type04 V1.05 can reduce the size by 25 bytes.
Suitable Products
Data Flash Libraries