Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Is the file code the accumulated value of the hexadecimal data?

Latest Updated:09/15/2006

Question:

Is the file code the accumulated value of the hexadecimal data? What is the difference between the file code and the previously used checksum value?

Answer:

The file code is the 32-bit length value of all the data in the mask file accumulated by 32-bit unsigned ASCII code. It is completely different from the EPROM checksum.
Suitable Products
Maskfile Converter
4500 Series ROM Ordering
720 Series ROM Ordering
38000 Series ROM Ordering
740/7450/7470 Series ROM Ordering
7600 Series ROM Ordering
7200 Series ROM Ordering
7770 Series ROM Ordering
M16C Family ROM Ordering
R8C Family ROM Programmed Shipment Ordering
QzROM Programmed Shipment Ordering
ASSP ROM Ordering
OSD Controller ROM Ordering