Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

What's the meaning of ".POOL" and ".NOPOOL" assembler source program?

Latest Updated:12/01/2009

Question:

What's the meaning of ".POOL" and ".NOPOOL" assembler source program?

Answer:

These are assembler directives which can control the behavior of the assembler.

".POOL" specify an output position of the literal pool in case of using the Automatic Literal Pool Generation Function. ".NOPOOL" to output the literal pool in case of using the Automatic Literal Pool Generation Function.

Suitable Products
C/C++ Compiler Package for SuperH Family