Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

What does -_msgoff specified as compiler option means?

Latest Updated:12/01/2014

Question:

I am using the CA78K0R compiler for RL78 and 78K0R products or the CA78K0 for 78K0 products. When I build a project, -_msgoff is specified as a compiler option.
What does this option specify?
Where is this option specified in CubeSuite+?

Answer:

Option -_msgoff is used to suppress the display of a startup message and cannot be controlled from CubeSuite+.
Note that the -_msgoff function is provided for use by CubeSuite+.
Suitable Products
C Compiler Package for RL78 and 78K Families
Compiler for RL78 Family and 78K0R [CA78K0R]
Assembler Package for 78K0R [RA78K0R]
Compiler for 78K0 [CA78K0]
Assembler Package for 78K0 [RA78K0]