Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

There is an error when I try to view information in the 78K/0 librarian

Latest Updated:12/01/2011

Question:

When I try to view information in the 78K/0 librarian, the following error is output.
What causes this error and how can it be handled?

|   78K/0 Series Librarian V3.10  [ 5 Mar 96]
|      Copyright (C) NEC Corporation 1990,1996
|   *l cl0.lib
|   F104 Illegal library file - different target chip (file : CL0.LIB)
|   *

Answer:

An error is output because no device file could be found when creating cl0.lib.
Try including the uPD78014's device file.

The uPD78014's device file can be downloaded from "Download Development Tools."

Suitable Products