Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

What does the error in the warning message as shown in output mean?

Latest Updated:12/01/2011

Question:

A static variable is declared in a function.
However, in the linker, an error and warning message is output as shown below:

ld850: warning: no LOAD segment exist for mapping input section ".sdata" in file "irtpr.o",

Answer:

This message indicates that the ".sdata" section does not exist in the link directive.
Add a .sdata section specification in the link directive.
Suitable Products
  • Was this article helpful?