What kinds of evaluation tools for Renesas CAN MCUs do you have?
Latest Updated:10/29/2005
Question:
What kinds of evaluation tools for Renesas CAN MCUs do you have?
Answer:
The following is a main evaluation tool for Renesas CAN MCUs.
Development tool-
- Hitachi ULSI Systems
・Micom Target System "Solution Engine" - VECTOR
・CAN Analyzer: CANalyzer
・CAN Oscilloscope: CANScope
・OSEK/VDX 2.0 compliant real-time multitasking operating system: osCAN etc. - Yokogawa Disital Computer Corporation
・CAN Flash Writer: C"arNET IMPRESS etc.
Suitable Products
R8C/22 |
R8C/23 |
M16C/6N4, M16C/6N5 |
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN |
M16C/1N |