Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

How do I change the granularity on the ThreadX Tick Clock in SSP?

Latest Updated:10/02/2016

Question:

The default granularity on the ThreadX clock Tick is 10ms. Is there a way for me to change this?

Answer:

The granularity of the Tick on ThreadX will be changeable via a CGC API call in a future SSP release. When the release date is available this post will be updated with that information. Once the API is available an example use will be show here.
Suitable Products
SSP