Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Is there a simpe SSP Example showing the use of TraceX?

Last Updated: 03/30/2016

Question:

Is there a simple example for SSP that shows how to use TraceX?

Answer:

The attached example project uses ThreadX Blinky to illustrate the use of TraceX.

https://knowledgebase.renesas.com/@api/deki/files/412/TraceX.zip

Here are the steps used to configure and run TraceX:

1. Add the ThreadX source. HAL/Common Modules>>New>>Framework>>RTOS>>ThreadX Source
2. Highlight ThreadX Source
3. Enable the following: Event Trace.
4. Run code
5. Suspend
6. Window>>Show View>>Memory
7. Click on green + icon. Type g_tx_trace_buffer into the address field.
8. Click Export icon Memory view. It is on the Memory tool bar towards the right with 1010 and an arrow up.
9. Save as: Format=RAW Binary, Length=65536. Filename=MyFavoriteTrace.trx
10. Double click on MyFavoriteTrace.trx (or open it within the TraceX)
11. DONE!

  • Was this article helpful?