Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

How do Install the USB Driver for the SSP e2 studio debug connection to a Synergy kit?

Latest Updated:10/04/2016

Question:

How do I install the debug interface USB driver for e2 studio and SSP to communicate to my Synergy Kit?

Answer:

The driver should be installed automatically when you install e2 studio and SSP. It will show up as the J-Link driver in the USB section of Windows Device manager.

J-Link.PNG

 

If for some reason it doesn't show up, you can install the driver manually from the Segger web site here: https://www.segger.com/jlink-software.html