Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

How does the use of Semi-Hosting impact my application?

Last Updated:03/01/2017

Question:

How does the use of semihosting impact my application?

Answer:

Semi-hosting disables interrupts for long periods of time. This cause issues like FIFO overflows and missed characters when also using SSP elements like HAL layer SCI drivers. Semi-hosting should not be used when real-time performance is required.
Suitable Products
SSP
  • Was this article helpful?