Skip to main content
Renesas India - Knowledgebase

Is the drive on output pins that require specific levels for a standard (like QSPI) automatically created for me when I add the module?

Latest Updated:10/04/2016


Is the drive on an output pin automatically configured correctly for the standard the pin is being used with? For example, on QSPI is the output drive set correctly when I add the module in SSP?



From SSP v1.1.0-alpha.1 onwards, all Synergy project templates in e2 studio enable the QSPI pins (and other pins) with the required drive strength (per MCU User Manual) via the associated *.pincfg file. What we CAN'T do at this point is assign this drive strength automatically when a peripheral is first enabled by the user in a blank *.pincfg (or if it is disabled an then re-enabled). This is a limitation in the pin configurator plug-in and there is no current plan to correct this.