Where can I find the completed telnet project for the console swap demo on the SK-S7G2 Kit?
Latest Updated:10/13/2016
Question:
Where can I find the completed Telnet version of the console swap demonstration?
Answer:
The completed project, in Synergy Import format is attached below. It uses the 192.168.0.0 default setting for the Ip address on the kit and was tested using a 192.168.0.100 IP address on the PC Ethernet Adaptor.
https://knowledgebase.renesas.com/@api/deki/files/422/ConsoleSwapEnet.zip