Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Where can I find documentation for the new DK-S124 kit?

Latest Updated:09/15/2016

Question:

Where can I find the documentation for the DK-S124 Kit?

Answer:

The DK-S124 documentation will be located on the Synergy Tools and Kits page on the Documentation Tab. Board design file are located on the Downloads tab, just like for all other Kits.

https://www.renesas.com/products/synergy/tools-kits.html 

The docs are not available at the time of this post however, so the Schematic has been made available here till the full doc and download sets are available on the Tools and Kits page.

DKS1_02a.pdf

Suitable Products
DK-S124