Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Where can I find the user guide for NetX features like DNS, FTP, HTTP, BSD, DCHP, SNTP and Telnet?

Latest Updated:10/13/2016

Question:

Where can I find the User's Manuals for NetX features like DNS, FTP, TFTP, HTTP, BSD, DCHP, SNTP and Telnet?

Answer:

You can find them on the Renesas Synergy Software web page here: https://www.renesas.com/produc...software.html

Just select the Documentation tab and check User's Manual: Software then click Search. It will bring up all the NetX related User's Manuals (as well as other Synergy software manuals).