Skip to main content
Renesas India - Knowledgebase

Where do I find Technical Updates for Synergy MCUs?

Latest Updated:10/13/2016


Where do I find the Technical Updates for Synergy MCUs?


You can find Technical Updates by navigating to the MCU page of the MCU of interest and selecting the Documentation Tab. One of the filter choices is Technical Update. Check that box and do a Search. All associated Technical Updates will appear. An example is shown below from the S1 Series page: 

Suitable Products
Synergy MCUs