Skip to main content
Renesas India - Knowledgebase

r_dac8 Module Guide Resources

Last Updated:11/20/2017


Where can I find the references to module guide resources for the DAC8 HAL module on r_dac8?


Information on the module guide itself and the associated resources and known issues are available here.


The DAC8 HAL module is a high-level API for digital-to-analog conversion applications implemented on r_dac8. The DAC8 HAL module supports an 8-bit D/A converter (DAC8) peripheral on Synergy S128 MCUs.

The DAC8 HAL module supports the following features:

  • Available on the Synergy S128 MCU
  • 8-Bit D/A Converter- three channels
  • Left-Justified or Right-Justified Input Data Format
  • Synchronization with the Analog-to-Digital Converter (ADC) module
  • Multiple Operation Modes
    • Normal
    • Real-Time (Event Link)
    • Charge Pump Control

Module Guide

The DAC8 HAL module guide is targeted for SSP 1.2.0 and above and the SK-S7G2 Kit.

The most recent versions of the DAC8 HAL module guide application note, application project and import guide are available here.

Module Guide Resources

Content will be provided as it becomes available

Known issues

  • Refer to the SSP release notes for known issues, available here.
  • Was this article helpful?